frexp


Divide floating-point number into mantissa and power

[Classification]

Mathematical library

[Syntax]

#include <math.h>

double frexp(double val, int *exp);

[Return value]

Returns mantissa m.

frexpf sets 0 to *exp and returns 0 if val is 0.

If val is +, frexpf returns zero and sets macro EDOM to global variable errno.

[Description]

This function expresses val of double type as mantissa m and the pth power of 2. The resulting mantissa m is 0.5 <= | x | < 1.0, unless val is zero. p is stored in *exp. m and p are calculated so that val = m * 2 p.