Convert floating-point number to power
double ldexp(double val, int exp);
Returns the value calculated byval x 2 exp.
If an underflow or overflow occurs as a result of executing ldexpf, macro ERANGE is set to global variable errno. If an underflow occurs, ldexpf returns an denormal number. If an overflow occurs, it returns HUGE_VAL.
This function calculates val x 2 exp.