Arc cosine
[Classification]
Mathematical library
[Syntax]
#include <math.h>
double  acos(double x);
[Return value]
Returns the arc cosine of x.  The returned value is in radian and in a range of 0 to .
If x is not between -1 and 1, a Not a Nuber(NaN) is returned, and macro EDOM is set to global variable errno.
[Description]
This function calculates the arc cosine of x.  Specify x as, -1<= x <= 1.