This dialog box sets filter conditions on analysis information which is displayed as the CPU usage status, in the Analysis information table area on the Analysis Result panel.
The following items are explained here.
Click on |
This area consists of the following two combo boxes.
Sets the comparison value (numerical value or character string) for filtering.
Up to 2048 characters can be input to this combo box.
Selects a filter condition for the comparison value which is set in the Combo box (left side).
This area consists of the following two buttons.
Sets the logic condition that "both filter conditions set in the 1st filter condition setting area and 2nd filter condition setting area are satisfied".
Sets the logic condition that "either of the filter conditions set in the 1st filter condition setting area and 2nd filter condition setting area is satisfied".
This area consists of the following two combo boxes.
Sets the comparison value (numerical value or character string) for filtering.
Up to 2048 characters can be input to this combo box.
Selects a filter condition for the comparison value set in the Combo box (left side).
Filters the analysis information to be displayed in the Analysis information table area on the Analysis Result panel, according to the filter condition set in this dialog box. |
|