3.2.7 Clock Serial Interface G

Below is a list of API functions output by the Code Generator for clock serial interface G use.

Table 3.7

API Functions: [Clock serial interface G]

API Function Name

Function

R_CSIGm_Create

Performs initialization necessary to control the clock serial interface G functions.

R_CSIGm_Create_UserInit

Performs user-defined initialization relating to the clock serial interface G functions.

r_csigm_interrupt_receive

Performs processing in response to the CSIG reception interrupt.

r_csigm_interrupt_error

Performs processing in response to the CSIG error interrupt.

r_csigm_interrupt_send

Performs processing in response to the CSIG communication interrupt.

r_csigm_callback_receiveend

Performs processing in response to the CSIG reception interrupt.

r_csigm_callback_sendend

Performs processing in response to the CSIG communication interrupt.

r_csigm_callback_error

Performs processing in response to the CSIG error interrupt.

R_CSIGm_Start

Sets CSIG communication to standby mode.

R_CSIGm_Stop

Ends CSIG communication.

R_CSIGm_Send

Start CSIG data transmission.

R_CSIGm_Receive

Start CSIG data reception.