3.2.11 Window Watchdog Timer

Below is a list of API functions output by the Code Generator for window watchdog timer use.

Table 3.11

API Functions: [Window watchdog timer]

API Function Name

Function

R_WDTm_Create

Performs initialization necessary to control the watchdog timer functions.

R_WDTm_Create_UserInit

Performs user-defined initialization relating to the watchdog timer functions.

r_wdtm_interrupt

Performs processing in response to the interval interrupt.

R_WDTm_Restart

Clears the watchdog timer counter and resumes counting.