3.2.25 Stand-By Controller

Below is a list of API functions output by the Code Generator for stand-by controller use.

Table 3.25

API Functions: [Stand-By Controller]

API Function Name

Function

R_STBC_Start_Stop_Mode

Start stand-by (STOP mode).

R_STBC_Prepare_Stop_Mode

Performs user-defined processing relating to the preparation to start stand-by (STOP mode).

R_STBC_Start_Deep_Stop_Mode

Start stand-by (DeepSTOP mode).

R_STBC_Prepare_Deep_Stop_Mode

Performs user-defined processing relating to the preparation to start stand-by (DeepSTOP mode).

R_STBC_Deep_Stop_Loop

Performs wait processing of stand-by (DeepSTOP mode).

R_STBC_Prepare_Stop_Mode_Set_Peripheral

Performs user-defined processing relating to the preparation (stop peripheral) to start stand-by (STOP mode).

R_STBC_Prepare_Stop_Mode_Set_Interrupt

Performs user-defined processing relating to the preparation (interrupt control register) to start stand-by (STOP mode).

R_STBC_Prepare_Stop_Mode_Set_Clock_Mask

Performs user-defined processing relating to the preparation (set the clock stop mask register) to start stand-by (STOP mode).

R_STBC_Prepare_Stop_Mode_Set_Clock_Source

Performs user-defined processing relating to the preparation (oscillate or stop each clock source) to start stand-by (STOP mode).

R_STBC_Prepare_Deep_Stop_Mode_Set_Peripheral

Performs user-defined processing relating to the preparation (stop peripheral) to start stand-by (DeepSTOP mode).

R_STBC_Prepare_Deep_Stop_Mode_Set_Interrupt

Performs user-defined processing relating to the preparation (interrupt control register) to start stand-by (DeepSTOP mode).