Renesas Electronics
Below is a list of API functions output by the Code Generator for Delta-Sigma AD converter use.
Table 3.20
API Functions: [Delta-Sigma AD converter]
API Function Name
Function
R_DSADC_Create
Performs initialization necessary to control the ΔΣ A/D converter functions.
R_DSADC_Create_UserInit
Performs user-defined initialization relating to the ΔΣ A/D converter functions.
r_dsadc_error_interrupt
Performs processing in response to the ΔΣ A/D error interrupt.
R_DSADC_SyncStart
Starts ΔΣ AD conversion set as enable AD synchronization start.
R_DSADCm_Start
Starts ΔΣ A/D conversion.
R_DSADCm_Stop
Ends ΔΣ A/D conversion.
R_DSADCm_GetResult
Reads the results of ΔΣ A/D conversion.