Renesas Electronics
R_SCIn_IIC_StartCondition
Sends the start bit.
Remark
This API function is called as the internal function of R_SCIn_IIC_Master_Send and R_SCIn_IIC_Master_Receive.
[Syntax]
void R_SCIn_IIC_StartCondition ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]