r_scin_transmit_interrupt


Performs processing in response to the transmit-data-empty interrupts.

Remark

This API function is called to run interrupt processing for the transmit-data-empty interrupts.

[Syntax]

static  void    r_scin_transmit_interrupt ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.