r_scin_callback_receiveend


Performs processing in response to the receive-data-full interrupts.

Remark

This API function is called as the r_scin_receive_interrupt callback routine.

[Syntax]

static  void    r_scin_callback_receiveend ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.