Performs processing in response to the receive-data-full interrupts.
Remark  | This function is called to run interrupt processing for the receive-data-full interrupts.  | 
 
[Syntax]
static  void    r_scin_receive_interrupt ( void ); 
 | 
 
Remark  | n is the channel number.  | 
 
[Argument(s)]
None.
[Return value]
None.