Renesas Electronics
r_scin_callback_receiveerror
Performs processing in response to the receive error interrupts.
Remark
This API function is called as the r_scin_receiveerror_interrupt callback routine.
[Syntax]
static void r_scin_callback_receiveerror ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]