BSR

Relative subroutine branch

BSR

Branch to SubRoutine


[Syntax]

BSR(.length) src

 

[Operation]

SP = SP - 4;

*SP = ( PC + n ) *;

PC = PC + src;

Notes 1.

1. (PC + n) is the address of the instruction following the BSR instruction.

Notes 2.

2. "n" indicates the code size. For details, refer to "Instruction Format".

 

[Function]

This instruction executes a relative branch to destination address specified by src.

 

[Instruction Format]

Syntax

Processng Size

src

Range of pcdsp / Rs

Code size

(Byte)

BSR(.length) src

W

pcdsp:16

-32768≦pcdsp≦32767

3

A

pcdsp:24

-8388608≦pcdsp≦8388607

4

L

Rs

-2147483648≦Rs≦2147483647

2

[Flag Change]

This instruction does not affect the states of flags.

[Description Example]

BSR label1

BSR.A label2

BSR R1

BSR.L R2

 

Note

For the RX Family assembler manufactured by Renesas Technology Corp., enter a destination address specified by a label or an effective address as the displacement value (pcdsp:16, pcdsp:24). The value of the specified address minus the address where the instruction is allocated will be stored in the pcdsp section of the instruction.

BSR label

BSR 1000h