FADD

Floating-point addition

FADD

Floating-point ADD


[Syntax]

FADD src, dest

 

[Operation]

FADD src, dest

 

[Function]

-

This instruction adds the single-precision floating-point numbers stored in dest and src and places the result in dest. Rounding of the result is in accord with the setting of the RM[1:0] bits in the FPSW.

-

Handling of denormalized numbers depends on the setting of the DN bit in the FPSW.

-

The operation result is +0 when the sum of src and dest of the opposite signs is exactly 0 except in the case of a rounding mode towards -?. The operation result is -0 when the rounding mode is towards -?.

 

[Instruction Format]

Syntax

Processng Size

src

dest

Code size

(Byte)

FADD src, dest

L

#IMM:32

Rd

7

L

Rs

Rd

3

L

[Rs].L

Rd

3

L

dsp:8[Rs].L

Rd

4

L

dsp:16[Rs].L

Rd

5

[Flag Change]

Flag

C

Z

S

O

CV

CZ

CU

CX

CE

FV

FO

FZ

FU

FX

Change

–

 

 

–

 

 

 

 

 

 

 

–

 

 

Conditions

Z : The flag is set if the result of the operation is +0 or -0; otherwise it is cleared.

S : The flag is set if the sign bit (bit 31) of the result of the operation is 1; otherwise it is cleared.

CV ::The flag is set if an invalid operation exception is generated; otherwise it is cleared.

CO : :The flag is set if an overflow exception is generated; otherwise it is cleared.

CZ : :The value of the flag is always 0.

CU ::The flag is set if an underflow exception is generated; otherwise it is cleared.

CX ::The flag is set if an inexact exception is generated; otherwise it is cleared.

CE : :The flag is set if an unimplemented processing is generated; otherwise it is cleared.

FV : :The flag is set if an invalid operation exception is generated, and otherwise left unchanged.

FO : :The flag is set if an overflow exception is generated, and otherwise left unchanged.

FU : :The flag is set if an underflow exception is generated, and otherwise left unchanged.

FX : :The flag is set if an inexact exception is generated, and otherwise left unchanged.

Note

The FX, FU, FO, and FV flags do not change if any of the exception enable bits EX, EU, EO, and EV is 1. The S and Z flags do not change when an exception is generated.

 

[Description Example]

FADD R1, R2

FADD [R1], R2