SUB

Subtraction without borrow

SUB

SUBtract


[Syntax]

(1)SUB src, dest

(2)SUB src, src2, dest

 

[Operation]

(1)dest = dest - src;

(2)dest = src2 - src;

 

[Function]

-

(1)This instruction subtracts src from dest and places the result in dest.

-

(2)This instruction subtracts src from src2 and places the result in dest.

 

[Instruction Format]

Syntax

Processng Size

src

src2

dest

Code size

(Byte)

(1)SUB src, dest

L

#UIMM:4

–

Rd

2

L

Rs

–

Rd

2

L

[Rs].memex

–

Rd

2 (memex == UB)

3 (memex != UB)

L

dsp:8[Rs].memex

–

Rd

3 (memex == UB)

4 (memex != UB)

L

dsp:16[Rs].memex

–

Rd

4 (memex == UB)

5 (memex != UB)

(2)SUB src, src2, dest

L

Rs

Rs2

Rd

3

[Flag Change]

Flag

C

Z

S

O

Change

 

 

 

 

Conditions

C : The flag is set if an unsigned operation produces no overflow; otherwise it is cleared.

Z : The flag is set if dest is 0 after the operation; otherwise it is cleared.

S : The flag is set if the MSB of dest after the operation is 1; otherwise it is cleared.

O : The flag is set if a signed operation produces an overflow; otherwise it is cleared.

 

[Description Example]

SUB #15, R2

SUB R1, R2

SUB [R1], R2

SUB 1[R1].B, R2

SUB R1, R2, R3