FMUL

Floating-point multiplication

FMUL

Floating-point MULtiply


[Syntax]

FMUL src, dest

 

[Operation]

dest = dest * src;

 

[Function]

-

This instruction multiplies the single-precision floating-point number stored in dest by that stored in src and places the result in dest. Rounding of the result is in accord with the setting of the RM[1:0] bits in the FPSW.

-

Handling of denormalized numbers depends on the setting of the DN bit in the FPSW.

-

The accumulator (ACC) is used to perform the function. The value of ACC after executing the instruction is undefined.

 

[Instruction Format]

Syntax

Processng Size

src

dest

Code size

(Byte)

FMUL src, dest

L

#IMM:32

Rd

7

L

Rs

Rd

3

L

[Rs].L

Rd

3

L

dsp:8[Rs].L

Rd

4

L

dsp:16[Rs].L

Rd

5

[Flag Change]

Flag

C

Z

S

O

CV

CZ

CU

CX

CE

FV

FO

FZ

FU

FX

Change

–

 

 

–

 

 

 

 

 

 

 

 

 

 

Conditions

Z : The flag is set if the result of the operation is +0 or -0; otherwise it is cleared.

S : The flag is set if the sign bit (bit 31) of the result of the operation is 1; otherwise it is cleared.

CV : The flag is set if an invalid operation exception is generated; otherwise it is cleared.

CO : The flag is set if an overflow exception is generated; otherwise it is cleared.

CZ : The flag is set if a division-by-zero exception is generated; otherwise it is cleared.

CU : The flag is set if an underflow exception is generated; otherwise it is cleared.

CX :The flag is set if an inexact exception is generated; otherwise it is cleared.

CE :The flag is set if an unimplemented processing exception is generated; otherwise it is cleared.

FV :The flag is set if an invalid operation exception is generated; otherwise it does not change.

FO :The flag is set if an overflow exception is generated; otherwise it does not change.

FZ :The flag is set if a division-by-zero exception is generated; otherwise it does not change.

FU :The flag is set if an underflow exception is generated; otherwise it does not change.

FX :The flag is set if an inexact exception is generated; otherwise it does not change.

Note

The FX, FU, FZ, FO, and FV flags do not change if any of the exception enable bits EX, EU, EZ, EO, and EV is 1. The S and Z flags do not change when an exception is generated.

 

[Description Example]

FMUL R1, R2

FMUL [R1], R2