[Microcontroller Information] tab


This tab shows the detailed information on microcontrollers configured in the project, categorized by the following and the configuration can be changed.

 

(1) [File Information]

(2) [Microcontroller Information]

(3) [IOR Display Type] [RH850]

(4) [Notes]

Figure A.14

Property Panel: [Microcontroller Information] Tab

[Description of each category]

(1)

[File Information]

The detailed information on the file is shown.

File name

Displays device file name.

Default

Device file name

How to change

Changes not allowed

Absolute path

Displays the absolute path of the device file.

Default

The absolute path of the device file

How to change

Changes not allowed

(2)

[Microcontroller Information]

The detailed information on microcontrollers is displayed and their configuration can be changed.

Microcontroller name

Displays microcontrollers to use in the project or the subproject.

Default

Microcontrollers used in the main project or the subproject

How to change

Changes not allowed

Nickname

Displays the nickname of the microcontroller to use.

Default

The nickname of the microcontroller to use

How to change

Changes not allowed

File version

Displays the device file version of the microcontroller to use.

Default

The device file version of the microcontroller to use

How to change

Changes not allowed

Bank size [KBytes]

Displays the bank size of the microcontroller being used in Kbytes, as a decimal number.

Note that this property is only shown for microcontrollers with a memory bank.

Default

The bank size recorded in your microcontroller's device file

How to change

Changes not allowed

Internal ROM size [KBytes]

Displays internal ROM size [KBytes]of the microcontroller to use in decimal number.

Default

Internal ROM size of the microcontroller to use

How to change

Changes not allowed

Internal RAM size [Bytes]

Displays internal RAM size [KBytes] of the microcontroller to use in decimal number.

Default

Internal RAM size of the microcontroller to use

How to change

Changes not allowed

Reset vector address

This is the reset vector address of the microcontroller to use.

See the user's manual of the device for the reset vector address.

Note that this property is displayed when the device has PE1 or is a single-core device.

Default

The peculiar value for the target device

How to change

Directly enter in the text box.

Restriction

0 to FFFFFFFF (hexadecimal number without 0x)

Reset vector address of PEn

This is the reset vector address of PEn of the microcontroller to use (n: core number).

See the user's manual of the device for about the reset vector address.

Note that this property is displayed when the device has PE1.

Default

The peculiar value for the target device

How to change

Directly enter in the text box.

Restriction

0 to FFFFFFFF (hexadecimal number without 0x)

(3)

[IOR Display Type] [RH850]

The detailed information on the IOR display type is shown.

IOR display type

Displays the IOR display type of the project.

Default

IOR display type of the project

How to change

Changes not allowed

(4)

[Notes]

The detailed information on records is displayed and their configuration can be changed.

Memo

Add memos to the microcontroller information.

The memo is added one item in one line.

The added memos are displayed as subproperty.

Default

Memo [Number of items]

How to change

Edit by the Text Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can use a text box directly enter the text.

Restriction

Up to 256 characters

Up to 256 characters are allowed.