Renesas Electronics
r_atuiv_timerknm_callback_ocrc
Performs processing in response to the OCRCnm register interrupt.
Remark
This API function is called as the callback routine of interrupt process r_atuiv_timerknm_interrupt corresponding to the OCRCnm register interrupt.
[Syntax]
void r_atuiv_timerknm_callback_ocrc ( void );
k is the timer kind, n is the unit number, m is the channel number.
[Argument(s)]
None.
[Return value]