r_atuiv_timerknm_fifo_datafull_interrupt


Performs processing in response to the FIFO data full interrupt.

[Syntax]

void    r_atuiv_timerknm_fifo_datafull_interrupt ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number.

[Argument(s)]

None.

[Return value]

None.