R_ATUIV_Timerknm_xpin_Output_Normal


Output of pin provides normal output.

[Syntax]

void    R_ATUIV_Timerknm_xpin_Output_Normal ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number, x is the output pin.

[Argument(s)]

None.

[Return value]

None.