R_ATUIV_Timerknm_Get_PWM_Measure_Value


Reads the PWM wave of measurement.

[Syntax]

void    R_ATUIV_Timerknm_Get_PWM_Measure_Value ( uint32_t * low_width, uint32_t * edge_width );

Remark

k is the timer kind, n is the unit number, m is the channel number.

[Argument(s)]

I/O

Argument(s)

Description

O

uint32_t * low_width;

Pointer to area in which to store the results of low level width

 

uint32_t * edge_width;

Pointer to area in which to store the results of edge interval count

[Return value]

None.