Renesas Electronics
R_ATUIV_Timerkn_Create_UserInit
Performs user-defined initialization relating to the each timer functions.
Remark
This API functions is called as the R_ATUIV_Timerkn_Create callback routine.
[Syntax]
void R_ATUIV_Timerk_Create_UserInit ( void );
void R_ATUIV_Timerkn_Create_UserInit ( void );
k is the timer kind, n is the unit number.
[Argument(s)]
None.
[Return value]