Renesas Electronics
Below is a list of API functions output by the Code Generator for DMAC use.
Table 3.5
API Functions: [DMAC]
API Function Name
Function
R_DMACn_Create
Performs initialization necessary to control the DMACn functions.
R_DMACn_Suspend
Suspend DMAC transfer for all channels.
R_DMACn_Resume
Resume DMAC transfer for all channels.
R_DMAC_Create_UserInit
Performs user-defined initialization relating to the DMACn functions.
r_dmacnm_interrupt
Performs processing in response to the DMACn channelm interrupt.
r_dmacnm_callback_transfer_completion
Performs processing in response to the DMAC transfer end interrupt.
r_dmacnm_callback_transfer_count_match
Performs processing in response to the DMAC transfer count match interrupt.
R_DMACnm_Create
Performs initialization necessary to control the DMACn channelm functions.
R_DMACnm_Start
Enables the DMACn channelm transfer.
R_DMACnm_Stop
Disables the DMACn channelm transfer.
R_DMACnm_Set_SoftwareTrigger
Generates the CMACn channelm transfer request..
R_DMACnm_Suspend
Suspend DMACn channelm transfer.
R_DMACnm_Resume
Resume DMACn channelm transfer.