3.2.6 DTS

Below is a list of API functions output by the Code Generator for DTS use.

Table 3.6

API Functions: [DTS]

API Function Name

Function

R_DTS_Create

Performs initialization necessary to control the DTS functions.

R_DTS_Create_UserInit

Performs user-defined initialization relating to the DTS functions.

R_DTS_Suspend

Suspend DTS transfer.

R_DTS_Resume

Resume DTS transfer/

R_DTS_All_Stop

Stop all DTS transfer.

R_DTSx_y_Stop_Interrupt

Stop DTS transfer interrupt.

R_DTSm_Create

Performs initialization necessary to control the DTS channel m functions.

R_DTSm_Start

Enables the DTS channel m transfer.

R_DTSm_Stop

Disables the DTS channel m transfer.

R_DTSm_Set_SoftwareTrigger

Generates the DTS channel m transfer request.

R_DTSm_Suspend

Suspend DTS channel m transfer.

R_DTSm_Resume

Resume DTS channel m transfer.

R_DTSm_Create_UserInit

Performs user-defined initialization relating to the DTS channel m functions.

r_dtsx_y_transfer_match_interrupt

Performs processing in response to the DTS transfer match interrupt.

r_dtsx_y_transfer_completion_interrupt

Performs processing in response to the DTS transfer completion interrupt.