3.2.17 Timer Option

Below is a list of API functions output by the Code Generator for timer option use.

Table 3.17

API Functions: [Timer option]

API Function Name

Function

R_TAPAm_Create

Performs initialization necessary to control the timer option functions.

R_TAPAm_Create_UserInit

Performs user-defined initialization relating to the timer option functions.

R_TAPAm_Start

Enables asynchronous Hi-Z control.

R_TAPAm_Stop

Disables asynchronous Hi-Z control.

R_TAPAm_Trigger_Start

Sets the Hi-Z control signal to the low level.

R_TAPAm_Trigger_Stop

Sets the Hi-Z control signal to the high level.