3.2.20 Delta-Sigma AD converter

Below is a list of API functions output by the Code Generator for Delta-Sigma AD converter use.

Table 3.20

API Functions: [Delta-Sigma AD converter]

API Function Name

Function

R_DSADC_Create

Performs initialization necessary to control the ΔΣ A/D converter functions.

R_DSADC_Create_UserInit

Performs user-defined initialization relating to the ΔΣ A/D converter functions.

r_dsadc_error_interrupt

Performs processing in response to the ΔΣ A/D error interrupt.

R_DSADC_SyncStart

Starts ΔΣ AD conversion set as enable AD synchronization start.

R_DSADCm_Start

Starts ΔΣ A/D conversion.

R_DSADCm_Stop

Ends ΔΣ A/D conversion.

R_DSADCm_GetResult

Reads the results of ΔΣ A/D conversion.