Renesas Electronics
Below is a list of API functions output by the Code Generator for timer array unit J use.
Table 3.16
API Functions: [Timer array unit J]
API Function Name
Function
R_TAUJn_Create
Performs initialization necessary to control the timer array unit Jn.
R_TAUJn_Create_UserInit
Performs user-defined initialization relating to the timer array unit Jn.
r_taujn_channelm_interrupt
Performs processing in response to the timer interrupt.
R_TAUJn_Channelm_Start
Starts the count for channel m.
R_TAUJn_Channelm_Stop
Ends the count for channel m.
R_TAUJn_Channelm_Get_PulseWidth
Reads the input pulse width of the timer.