Starts SCI reception (smart card interface mode).
This API function repeats SCI reception in byte units the number of times specified by the argument rx_num and then stores the received data in the buffer at the location specified by the argument rx_buf. |
When performing a SCI reception, R_SCIn_Start must be called before this API function is called. |
#include "r_cg_macrodriver.h" MD_STATUS R_SCIn_SmartCard_Receive ( uint8_t * const rx_buf, uint16_t rx_num ); |