Starts SCI slave transmission (simple SPI mode).
This API function repeats the byte-level SCI slave transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num. |
When performing a SCI slave transmission, R_SCIn_Start must be called before this API function is called. |
#include "r_cg_macrodriver.h" MD_STATUS R_SCIn_SPI_Slave_Send ( uint8_t * const tx_buf, uint16_t tx_num ); |