r_scin_callback_receiveerror


Performs processing in response to the receive error interrupts.

Remark

This API function is called as the r_scin_receiveerror_interrupt callback routine.

[Syntax]

static  void    r_scin_callback_receiveerror ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.