Renesas Electronics
r_scin_callback_transmitend
Performs processing in response to the transmit-end interrupts.
Remark
This API function is called as the r_scin_transmitend_interrupt callback routine.
[Syntax]
static void r_scin_callback_transmitend ( void );
n is the channel number.
[Argument(s)]
None.
[Return value]