R_SCIn_IIC_Master_Send


Starts SCI master transmission (simple I2C mode).

Remarks 1.

This API function handles SCI master transmission to the slave device at the address specified by the argument adr and the R/W#bit. SCI master transmission in byte units is repeated the number of times specified by the argument tx_num from the buffer at the location specified by the argument tx_buf.

Remarks 2.

This API function internally calls R_SCIn_IIC_StartCondition to handle processing to start SCI master transmission.

Remarks 3.

When performing a SCI master transmission, R_SCIn_Start must be called before this API function is called.

[Syntax]

#include    "r_cg_macrodriver.h"
void    R_SCIn_IIC_Master_Send ( uint8_t adr, uint8_t * const tx_buf, uint16_t tx_num );

Remark

n is the channel number.

[Argument(s)]

I/O

Argument

Description

I

uint8_t         adr;

Slave address

I

uint8_t * const tx_buf;

Pointer to a buffer storing the transmission data

I

uint16_t        tx_num;

Total amount of data to send

[Return value]

None.