Column Chooser dialog box


This dialog box is used to sort, show/hide the columns displayed on the Memory Mapping Profiler panel.

If the display in the panel has been customized, all of those customizations can be returned to the default state in this dialog box.

Figure A.29

Column Chooser Dialog Box

 

The following items are explained here.

[How to open]

-

On the Memory Mapping Profiler panel, click the button.

[Description of each area]

(1)

Item list area

This area displays a list of all columns that can be displayed on the Memory Mapping Profiler panel.

The display order of the columns in this list, and the state of check boxes, are the same as the current sort order and visible/hidden status in the panel.

 

This area has the following functions.

-

Rearrange the columns on the Memory Mapping Profiler panel

The columns displayed on the panel can be rearranged with the following method.

-

Drag the column displayed in this dialog box and drop it in the [Details of the selected memory mapping] area on the panel.

-

Specify display or non-display for columns on the Memory Mapping Profiler panel

The columns to be displayed on the panel can be set with either of the following methods.

-

Select the check box of a column displayed in this dialog box.

-

Drag a column displayed in this dialog box and drop it in the [Details of the selected memory mapping] area on the panel.

 

The columns not to be displayed on the panel can be set with the following method.

-

Cancel the selection of the check box of a column displayed in this dialog box.

[Function buttons]

Button

Function

Default

Resets the display order and visible/hidden settings for columns on the Memory Mapping Profiler panel to their default values.

Close

Closes this dialog box.