This dialog box is used to input and edit texts in multiple lines.
Figure A.19 | Text Edit Dialog Box (When Caller Supports Placeholders) |
Figure A.20 | Text Edit Dialog Box (When Caller Does Not Support Placeholders) |
The following items are explained here.
[How to open]
- | Select the property corresponding with this dialog box on the Property panel, and then click the [...] button. |
[Description of each area]
Edit texts in multiple lines.
By default, the current value of the area that this dialog box is called from is reflected in this area.
Remark | Up to 500 lines and 500 characters can be entered. Note that the upper limit value is differing depending on the area that this dialog box is called from.
When the input violates any restriction, the following message will be shown in the tooltip. |
|
|
More than maximum number of restriction in the property that called this dialog box characters cannot be specified. The current number of characters is displayed between brackets at the beginning of the line in excess of the limit.
|
The numbers of input characters exceeds the maximum number of restriction in the property that called this dialog box.
|
The list of placeholders which can be specified for the area that this dialog box is called from is displayed (ascending order).
Double click a row to surround the placeholder with percentage signs ("%"), and display it in [Text].
This area displays the placeholder.
The string is displayed after replacement with the placeholder.
This area displays the description of the placeholder.
Remark | The placeholders which can be specified differ depending on the area that this dialog box is called from.
For the specific placeholder, see the description of the area that this dialog box is called from. |
[Function buttons]
|
|
OK
|
Reflects the entered text to the text box that opened this dialog box and closes this dialog box.
|
Cancel
|
Does not reflect the entered text to the text box that opened this dialog box and closes this dialog box.
|
Help
|
Displays the help of this dialog box.
|