r_iicmn_interrupt

Performs processing in response to the simple IIC communication end interrupt INTIICmn.

Remark This API function is called as the interrupt process corresponding to the simple IIC communication end interrupt INTIICmn.

[Syntax]

CA78K0R Compiler

__interrupt static void r_iicmn_interrupt ( void );

CC-RL Compiler

static void __near r_iicmn_interrupt ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.