R_SAUm_Set_PowerOff

Halts the clock supplied to the serial array unit.

Remark Calling this API function changes the serial array unit to reset status.
For this reason, writes to the control registers (e.g. serial clock select register n: SPSn) after this API function is called are ignored.

[Syntax]

void R_SAUm_Set_PowerOff ( void );

Remark m is the unit number.

[Argument(s)]

None.

[Return value]

None.