R_UARTn_Create

Performs initialization necessary to perform the UART communication.

Remark This API function is used as an internal function of R_SAUm_Create.
For this reason, there is normally no need to call it from a user program.

[Syntax]

void R_UARTn_Create ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.