R_IICmn_StartCondition

Generates start conditions.

Remark This API function is used as an internal function of R_IICmn_Master_Send and R_IICmn_Master_Receive .
For this reason, there is normally no need to call it from a user program.

[Syntax]

void R_IICmn_StartCondition ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.