Performs processing in response to the UART reception error interrupt INTSREn.
Remark This API function is called as the callback routine of interrupt process r_uartn_interrupt_error corresponding to the UART reception error interrupt INTSREn.
[Syntax]
#include r_cg_macrodriver.h
static void r_uartn_callback_error ( uint8_t err_type );
Remark n is the channel number.
[Argument(s)]
I/O |
Argument |
Description |
O |
uint8_t err_type; |
Trigger for UART reception error interrupt 00000xx1B: Overrun error 00000x1xB: Parity error 000001xxB: Framing error |
[Return value]
None.