R_IT8bitm_Channeln_Create_UserInit

Performs user-defined initialization relating to the 8-bit interval timer.

Remark This API function is called as the R_IT8bitm_Channeln_Create callback routine.

[Syntax]

void R_IT8bitm_Channeln_Create_UserInit ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.