Renesas Electronics
Starts the count of the 8-bit interval timer.
[Syntax]
void R_IT8bitm_Channeln_Start ( void );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
None.
[Return value]