R_IT8bitm_Set_PowerOff

Halts the clock supplied to the 8-bit interval timer.

Remark Calling this API function changes the 8-bit interval timer to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

[Syntax]

void R_IT8bitm_Set_PowerOff ( void );

Remark m is the unit number.

[Argument(s)]

None.

[Return value]

None.