r_it8bitm_channeln_interrupt

Performs processing in response to the 8-bit interval timer interrupt INTITn0 or INTITn1.

Remark This API function is called as the interrupt process corresponding to the 8-bit interval timer interrupt INTITn0 or INTITn1.

[Syntax]

CA78K0R Compiler

__interrupt static void r_it8bitm_channeln_interrupt ( void );

CC-RL Compiler

static void __near r_it8bitm_channeln_interrupt ( void );

Remark m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.