r_uartfn_callback_idmatch

Performs processing in response to match ID parity.

Remark This API function is called as the callback routine of interrupt process r_uartfn_interrupt_error corresponding to the LIN-UART reception status interrupt INTLS (performed when ID parity has been matched).

[Syntax]

static void r_uartfn_callback_idmatch ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.