r_uartfn_interrupt_error

Performs processing in response to the LIN-UART reception status interrupt INTLS.

Remark This API function is called as the interrupt process corresponding to the LIN-UART reception status interrupt INTLS.

[Syntax]

CA78K0R Compiler

__interrupt static void r_uartfn_interrupt_error ( void );

CC-RL Compiler

static void __near r_uartfn_interrupt_error ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.