r_uartfn_interrupt_receive

Performs processing in response to the LIN-UART reception end interrupt INTLR.

Remark This API function is called as the interrupt process corresponding to the LIN-UART reception end interrupt INTLR.

[Syntax]

CA78K0R Compiler

__interrupt static void r_uartfn_interrupt_receive ( void );

CC-RL Compiler

static void __near r_uartfn_interrupt_receive ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.