Below is a list of API functions output by the Code Generator for asynchronous serial interface LIN-UART (UARTF) use.
Table 3.33 API Functions: [Asynchronous Serial Interface LIN-UART]
| 
 API Function Name  | 
 Function  | 
| 
 Performs initialization necessary to control the asynchronous serial interface LIN-UART (UARTF).  | |
| 
 Performs user-defined initialization related to the asynchronous serial interface LIN-UART (UARTF).  | |
| 
 Performs processing in response to the LIN-UART transmission end interrupt INTLT.  | |
| 
 Performs processing in response to the LIN-UART reception end interrupt INTLR.  | |
| 
 Performs processing in response to the LIN-UART reception status interrupt INTLS.  | |
| 
 Sets LIN communication to standby mode.  | |
| 
 Ends LIN communication.  | |
| 
 Halts the clock supplied to the asynchronous serial interface LIN-UART (UARTF).  | |
| 
 Starts UARTF data transmission.  | |
| 
 Starts UARTF data reception.  | |
| 
 Starts the data comparison.  | |
| 
 Ends the data comparison.  | |
| 
 Performs processing in response to the LIN-UART transmission end interrupt INTLT.  | |
| 
 Performs processing in response to the LIN-UART reception end interrupt INTLR.  | |
| 
 Performs processing in response to the LIN-UART reception status interrupt INTLS.  | |
| 
 Performs processing in response to detection of overrun error.  | |
| 
 Performs processing in response to detection of expansion bit.  | |
| 
 Performs processing in response to match of ID parity.  |