r_uartfn_interrupt_send

Performs processing in response to the LIN-UART transmission end interrupt INTLT.

Remark This API function is called as the interrupt process corresponding to the LIN-UART transmission end interrupt INTLT.

[Syntax]

CA78K0R Compiler

__interrupt static void r_uartfn_interrupt_send ( void );

CC-RL Compiler

static void __near r_uartfn_interrupt_send ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.