-  | The divh instructions of the device should be specified in the following formats.  | 
 
 
-  | In asrh, the following formats can also be used in addition to the above.  | 
 
 
-  | If the instruction is executed in syntax "divh imm, reg2", and the following expression is specified for imm, the assembler executes instruction expansion to generate multiple machine instructions.  | 
 
(a)  | Absolute expression having a value of other than 0 within the range of -16 to +15  | 
 
divh    imm5, reg 
 | 
mov     imm5, r1 
divh    r1, reg 
 | 
 
(b)  | Absolute expression exceeding the range of -16 to +15, but within the range of -32,768 to +32,767  | 
 
divh    imm16, reg 
 | 
movea   imm16, r0, r1 
divh    r1, reg 
 | 
 
(c)  | Absolute expression having a value exceeding the range of -32,768 to +32,767   | 
 
If all the lower 16 bits of the value of imm are 0
divh    imm, reg 
 | 
movhi   HIGHW(imm), r0, r1 
divh    r1, reg 
 | 
 
 
Else
divh    imm, reg 
 | 
mov     imm, r1 
divh    r1, reg 
 | 
 
(d)  | Relative expression having !label or %label, or that having $label for a label having a definition in the sdata/sbss-attribute section  | 
 
divh    !label, reg 
 | 
movea   !label, r0, r1 
divh    r1, reg 
 | 
divh    %label, reg 
 | 
movea   %label, r0, r1 
divh    r1, reg 
 | 
divh    $label, reg 
 | 
movea   $label, r0, r1 
divh    r1, reg 
 | 
 
(e)  | Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section  | 
 
divh    #label, reg 
 | 
mov     #label, r1 
divh    r1, reg 
 | 
divh    label, reg 
 | 
mov     label, r1 
divh    r1, reg 
 | 
divh    $label, reg 
 | 
mov     $label, r1 
divh    r1, reg 
 | 
 
 
-  | If the instruction is executed in syntax "divh imm, reg2, reg3", and the following expression is specified for imm, the assembler executes instruction expansion to generate one or more machine instructions.  | 
 
divh    0, reg2, reg3 
 | 
divh    r0, reg2, reg3 
 | 
 
(b)  | Absolute expression having a value of other than 0 within the range of -16 to +15  | 
 
divh    imm5, reg2, reg3 
 | 
mov     imm5, r1 
divh    r1, reg2, reg3 
 | 
 
(c)  | Absolute expression exceeding the range of -16 to +15, but within the range of -32,768 to +32,767  | 
 
divh    imm16, reg2, reg3 
 | 
movea   imm16, r0, r1 
divh    r1, reg2, reg3 
 | 
 
(d)  | Absolute expression having a value exceeding the range of -32,768 to +32,767  | 
 
If all the lower 16 bits of the value of imm are 0
divh    imm, reg2, reg3 
 | 
movhi   HIGHW(imm), r0, r1 
divh    r1, reg2, reg3 
 | 
 
 
Else
divh    imm, reg2, reg3 
 | 
mov     imm, r1 
divh    r1, reg2, reg3 
 | 
 
(e)  | Relative expression having !label or %label, or that having $label for a label having a definition in the sdata/sbss-attribute section  | 
 
divh    !label, reg2, reg3 
 | 
movea   !label, r0, r1 
divh    r1, reg2, reg3 
 | 
divh    %label, reg2, reg3 
 | 
movea   %label, r0, r1 
divh    r1, reg2, reg3 
 | 
divh    $label, reg2, reg3 
 | 
movea   $label, r0, r1 
divh    r1, reg2, reg3 
 | 
 
(f)  | Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section  | 
 
divh    #label, reg2, reg3 
 | 
mov     #label, r1 
divh    r1, reg2, reg3 
 | 
divh    label, reg2, reg3 
 | 
mov     label, r1 
divh    r1, reg2, reg3 
 | 
divh    $label, reg2, reg3 
 | 
mov     $label, r1 
divh    r1, reg2, reg3 
 |